Hello,
I want to know about Short to GND protection of TPS200D1-Q1.
Datasheet page2 ABSOLUTE MAXIMUM RATINGS ha following explanation.
But, no another explanation about short-circuit protection in the datasheet.
(2) For the MSOP (DGN) package option, the maximum VDD should be limited to 5 V if short-circuit protection is desired.
Block diagram on page4 has “Short Circuit detects Circuit” but no explanation.
Please answer if TPA2005D1-Q1 has Vo+/- short to GND protection.
And please explain operation details in case of it has short-circuit protection to GND.
Best Regards.