Hi,
I want to use UART communication, not LIN for PGA450. Would you please provide the required code settings?
In addition, please let me know when we use SPI communication.
Best Regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to use UART communication, not LIN for PGA450. Would you please provide the required code settings?
In addition, please let me know when we use SPI communication.
Best Regards,
Kato
Kato,
The TIDA-00151 UART Demo Firmware for PGA450-Q1 is available on the Software tab of the PGA450-Q1 product page. The TIDA-00151 UART Instructional provides guidelines on how to use this demo firmware. SPI communication is used for debug and development purposes, primarily for use with the PGA450Q1EVM-GUI. Refer to section 7.4.3 RESET of the PGA450-Q1 datasheet to read more about the limitations of the SPI interface.
Hi Akeem - san,
Thank you for the reply. Conversely, could customer control PGA450 by using only SPI communication ?
Best Regards,
Kato
Hi Akeem - san,
Thank you for the explanation. After all, customer is considering using only SPI since the interface is limited.
Is there any problem if customer wouldn't use UART or LIN for the simultaneous transfer ?
Best Regards,
Kato
Would it possible to run TOF logic at the external MCU as following way?
- Permanently put 8051 to RESET state and never use 8051.
- Control and drive PGA450 from external MCU through SPI interface to Transmit and Receive sound
- The external MCU read FIFO through SPI and get TOF
TIDA-00151 UART Demo Firmware for PGA450-Q1 v2.6 (Rev. C) link points to wrong download, Can you please post the correct link
Thanks
Dj
Dj,
Thank you for reporting this file linking error! I have reported the issue to our software logistics team, and will notify you when the download has been corrected.
FYI, we've recently updated the source code/firmware and instructional for the TIDA-00151 (also available as the PGA450Q1EVM-S).
The new demo UART instructional is integrated into the PGA450Q1EVM-S User's Guide at:
Dj,
Please check the link now. It should be working, with a price listing of $49.