Hi,
I have a problem of the overshoot at power up.
When the ADJ terminal is rised , it is the overshoot is as large as 6.5V.
Then ADJ is 5V , Iout is 25mA, Vin is 16V and output capacitor is 1uF.
For slew rate is high, it seems to output been reached over 6V before the softstart will work .
I think that output capacitor should be large.
How should I decide to do the size of the capacitor?
Best regards,