Hola,
We have a serious over heat issue about TPS79801-Q1, 50% production error rate by TPS79801-Q1 over heat that causes MSP430 internal flash data error.
After analysis and we found the power pad(thermal pad) solder paste is not good enough and it will causes device over heat and increased leakage current!
Does this thermal pad connected to the GND pin internally?why it causes increased leakage current by poor solder paste?
And I have measured the current at the output side from TPS79801-Q1, when device is at normal temperature and the output current is about 20mA,
but when I measured the over heat device and the output current is about 120mA!Is this caused by poor solder from thermal pad?