Hello,
Please answer following question from customer.
Please advise if TPA6211a1-Q1 has over current protection.
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Please answer following question from customer.
Please advise if TPA6211a1-Q1 has over current protection.
Best Regards.
Hello,
Please answer my previous question.
Also, please advise how many current will flow from VDD to VO when output is shorted to GND.
Best Regards.
Hello Clancy-san,
Thank you for your answer.
I’m sorry I forgot I have ever asked same question.
Your answer and link said that thermal shutdown will work when VO is shorted.
I tested the shutdown behavior using TPA6211A1 EVM and result is attached.
When I shorted VO- to GND, VO repeat high and 0V and it looks like repeating shutdown and wakeup.
When I sorted VO+ to VO-, VO repeat high and 0V and it looks like repeating shutdown and wakeup.
I also measured VDD current using current meter of DC power supply.
TPA6211A1-Q1 VO short to GND.pptx
Please advise is this working thermal shutdown.
Does TPA6211A1-Q1 continue shutdown while Tj is higher than 150C?
Best Regards.
Hello Clancy-san,
Thank you for your answer.
I tested thermal protection by short VO+ and VO- to GND during 10 to 15 minutes.
After above short test device was damaged.
VO+ output normal sign wave but VO- output 0V with no speaker.
VO+ and VO- output same phase sign wave with speaker, so I think VO- is floating.
Could you confirm that VO short to GND doesn’t damage the device because thermal protection protect the device.
Best Regards.
Hello Clancy-san,
According to your link (https://e2e.ti.com/support/amplifiers/audio_amplifiers/f/6/t/480904), José-san said “When the amplifier's outputs had a short circuit, I drove the output to 821 mVrms and got 960 mArms, after a few seconds the current dropped some mArms.”.
But when I tested output short to GND, I observed 0.86A to 0.6A VDD current and this current does not dropped to some mA.
Please confirm that VO short to GND doesn’t damage the device because thermal protection protect the device.
Best Regards.
Hello Clancy-san,
Thank you for your test.
I tested as following.
- Was there a load? ⇒6 ohm speaker
- Was there an input signal? ⇒apply 3Vp-p 1KHz sign wave to IN- of EVM, IN+ is connect to GND, so output is 6Vp-p differential.
- What was the VDD voltage? ⇒5V
I tested following short case.
Case-1: VO+ or VO- to GND
Case-2: VO+ and VO- to GND at the same time.
I continued to short during 5 minute and VDD current is decreased around 1.1A to 0.6A but it did not decrease significantly for Case-1 and Case-2.
Q1:
Does “Some mArms” of José-san’s answer means 3 or 4 mA?
Q2:
I don’t have another EVM to test short to GND.
Could you confirm that device is not damaged after your short test?
Best Regards.
Hello Clancy-san,
Thank you for your EVM short current information and test results.
Please let me known your few more test results.
Best Regards.