Several RESET related issues, interfaced to TMS570.
1. When the TPS65381 RESETs the TMS570, how can I read the TPS65381 to determine the cause of the REST?
2. While in DIAGNOSTIC Mode, the WD Counter is set/serviced to '0'; the TPS65381 is then changed to ACTIVE Mode, a RESET is immediately generated. Why would this happen and what can be done to prevent this RESET?
3. Related to 2, WD_RST_EN is set to 0, INIT routine for the TPS65381 is performed and without changing WD_RST_EN, a RESET is still generated. What would cause this RESET to occur?
4. When a SEQ_ERR occurs, is there a register in the TPS65381 to inform as to the data received?
~Leonard