Hello,
I'm not sure if this is the right forum, but there is an MSP430 on the PGA411-Q1 EVM, so let's start here.
Is it possible to control the PGA411-Q1 chip from an external MCU via the SPI bus, instead of using the on-board MSP430? I.e. once we checkout the resolver operation using the supplied GUI and MSP430 firmware, we would like to use the same board, but drive the resolver chip from our own microcontroller via the SPI bus.
Thanks,
Chuck