Hi all,
I'm looking to put together an high speed ADC and DSP for some embedded prototyping. There are a lot of eval kits for ADCs, and a lot for DSPs, but none seem to go directly together.
The ADC spec I'm looking for is 2ch, 40MSPS, 12bit performance. It only needs to take data in short bursts (<5ms) then let the DSP process on the data for a bit.
So, my question is how to make the hardware connection? I understand about LVDS or other serial standards, but I'm not sure how to tell if a DSP can handle a CMOS parallel output from an ADC. Or if that is even a good idea.
My second question is, if the ADC and DSP can come together using LVDS or CMOS parallel, is there a ready-made evaluation solution for this? Or a couple of them that can be rigged together? I'd really like to avoid making, assembling and debugging my own PCB.
I'm hoping to avoid using a FPGA to reduce complexity, because the ready to go features of DSP (like GPIO/SPI/I2C to control my peripheral) are really nice.
Something like the 12.5MSPS Delfino would be perfect aside from the underspecced ADC, and I got one just in case I can reduce the demand on the ADC on the peripheral side.
Thanks for your time,
Paul