Hi TI,
I have the following questions.
Would you please reply them?
<Customer System>
CMOS Camera (1ch) => DS90UB953-Q1(Serializer) => DS90UB9xx (Deserializer) => SoC(System on chip)
-1lane/MIPI CSI2 Out put -Need to Parallel data out
-VGA Size(640x480) (substitute:MIPI CSI2 Out)
-Color: Black & white
-Raw Data/ 8 or 10bit
-60fps
<Questions>
For Serializer
Q1. Though DS90UB953 has 4ch data input, Can I use only 1ch input ?
Q2.If it is OK, how much is the band width of 1lane? 1.5Gbps ?
For Derializer
Q3.Could you inform me of deserializer which can connect to DS90UB953, and has Parallel Output?
(In addition, the device must satisfy the system mentioned above.)
Q4.Can DS90UB954-Q1 handle data of RAW 8bit or 10bit?
For Serializer/Derializer
Q5. The MIPI output from a CMOS camera may become burst data (not continuation).
The MIPI clock may become intermittent, too.
In this case, can I use it without a problem?
Thank you for your help.
Best Regards,Orobianco