Hi, Team
A Car-OEM customer GAC is evaluating TPS65381-Q1 for their EPB system. They have questions on it.
1. There are two modes of watchdog in TPS65381-Q1: Trigger Mode or Question and Answer Mode.
Customer need to turn off all the watchdog, when they program the software code to MCU. Because there is no software in MCU before program, and MCU can not feed the watchdog.
Can the watchdog in TPS65381-Q1 be turned off without MCU control through SPI? How can we do it?
2. When there is over temperature condition, bit 0~2 of SAFETY_STAT_1 Register will be 1. When over temperature condition remove, the bit return to 0.
over temperature condition occur --> power output disable and related register bits set to 1 --> MCU power down (MCU can not read out the over temperature condition) --> when over temperature condition remove --> MCU power up but the related register bits return to 0
How can MCU log the over temprature condition?
Thanks
Kevin