Hi all,
we are designing an equipment that is going to be plug in trucks. In our design, we are going to use two regulators, one for dropping the input voltage from 12/24v to 5 V, and a second regulator, a LP5900SD-3.3 for dropping again from 5 V to 3.3 V with low noise, because at that point we need a low noise supply.
Another point to consider, is that the truck supply (is made for very big trucks) is not stable, due to transient when the trucks ignites, and the cable that we use to connect our equip from the truck battery is quite long (10 meters).
Taking that information in consideration, I'm not sure about which capacitor use at the input of the TPS7, because the datasheets says bigger than 0.1 uF, but the power supply recommendations says that if the input supply is far from the LDO, 10 uF electrolytic is recommended. If I have to use 10 uF, ceramic is not possible (due to capacitance / DC vias derating), electrolytic lifetime is very short for our application, so the only option is poly tantalum. But if we can use lower capacitance, we have more option.
Thanks for your help,
Regards,