Hi guys,
can you let me know the Average and max current on VCC and VCCSW on the PGA411-Q1?
Regards,
Jon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi guys,
can you let me know the Average and max current on VCC and VCCSW on the PGA411-Q1?
Regards,
Jon
Hi,
thank you for the fast replay.
For the first design it is enough, if you could tell me the worst case currents.
Thanks,
Matthias
Data taken from PGA411EVM:
4Vrms Boost voltage set to 12V (standard)
Load resistance 43 ohms Load:101.480 mArms DC offset: 2V Gain:1.9
Supply Current: 294 mA
Load resistance 75 ohms Load: 59.943 mArms DC offset: 2V Gain: 1.9
Supply Current: 193 mA
7Vrms Boost voltage set to 15V (standard)
Load resistance: 74 Ohms Load: 102.158 mArms DC offset:2V Gain:1.9
Supply Current: 366 mA
Load resistance 132 ohms Load: 60.196 mArms DC offset: 2V Gain: 1.9
Supply Current: 235 mA
For the 4Vrms setting, the boosted voltage selected was 12V which is expected for standard operation. The boosted voltage is 15V for the 7Vrms setting and was chosen for the same reason. The DC offset and Gain were chosen to be at the maximum setting to show worst case scenario on the supply current draw.
The max load current was chosen to be 145 mApeak (or about 102.53 mArms) due to the maximum allowed output current specified by the datasheet. A reference point of 85mApeak (or about 60.1mArms) was used to show the difference on the supply current draw.
Conclusion:
From the data above, it can be seen the maximum supply current draw occurs at 7Vrms with a boosted voltage of 15V. Supply Current at this setting is 366mA.
Side note:
The supply current can be minimized by adjusting the boosted voltage; this boosted voltage controls the headroom of the output and should be chosen to avoid the output from clipping. Therefore to minimize the supply current draw, the minimal voltage allowable to avoid clipping should be used.
The DC offset behaves the same way but affects the foot room of the output (should be chosen to to be lowest possible to avoid clipping and minimize supply current draw). This parameter does not affect the supply current AS MUCH as the boost voltage setting.