Hi,
Does MCSDK-HPC related packages be compatible Debian Linux distribution? From the wiki I only see it is tested on Ubuntu, but just wanna make sure if it works on Debian.
Thanks
Cheng
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Does MCSDK-HPC related packages be compatible Debian Linux distribution? From the wiki I only see it is tested on Ubuntu, but just wanna make sure if it works on Debian.
Thanks
Cheng
I tried on Debian 7 Jessie, but the glibc on it is too old, with version 2.13, but the cl6x requires the glibc to be >=2.14.
So I suppose if you use Debian 7, you'd better use the "test" repo on Debian to upgrade the glibc, then it should work.
Just FYI.