Hi, all
After I install the version of MCSDK-HPC_03_00_00_18, and run the project example(ECPY_example) located in .../ti/blas_03_11_00_00/blas/example/Setup_ECPY/app/build/ccs, It can run correctly, but I have a question about the ECPY_example.map file: why the section .far occupy so big memory size?
the example matrix size is 2×3 and 3×2.
my hardware is EVM6678L, and the 4188.blas-lib-3.11.0.pdf is about run instruction of ECPY_example provide by Ming Wei.
and if I want to accurate big matrix-matrix multiply(like matrix order is 1000 and element is float type), DDR3 there no more room for my original matrix, what should I do?
Thanks!
Mike