Hi,
We have a custom board with 66AK2H14 processor . I am trying to perform srio enumeration from ARM (66AK2H14) and using kernel version 4.4.12 from latest SDK.
My port is not getting trained . Attached the log,
[ 0.360393] keystone-rapidio 2900000.rapidio: KeyStone RapidIO driver v1.4 [ 0.360452] keystone-rapidio 2900000.rapidio: missing "rx-queue" parameter for mbox 0, using qpend [ 0.360463] keystone-rapidio 2900000.rapidio: missing "tx-completion-queue" parameter for mbox 0, using qpend [ 0.360469] keystone-rapidio 2900000.rapidio: missing "tx-garbage-queue" parameter for mbox 0, using qpend [ 0.360485] keystone-rapidio 2900000.rapidio: missing "rx-queue" parameter for mbox 1, using qpend [ 0.360495] keystone-rapidio 2900000.rapidio: missing "tx-completion-queue" parameter for mbox 1, using qpend [ 0.360501] keystone-rapidio 2900000.rapidio: missing "tx-garbage-queue" parameter for mbox 1, using qpend [ 0.360573] keystone-rapidio 2900000.rapidio: using K2 SerDes [ 0.360623] keystone-rapidio 2900000.rapidio: initializing 5.00 Gbps interface with port configuration 4 [ 0.574140] keystone-rapidio 2900000.rapidio: packet forwarding disabled [ 6.814111] keystone-rapidio 2900000.rapidio: initializing lane mask 0xf for port 0 [ 6.924079] keystone-rapidio 2900000.rapidio: port 0 lane mask 0xf is not OK [ 9.934157] keystone-rapidio 2900000.rapidio: initializing lane mask 0xf for port 0 [ 10.044108] keystone-rapidio 2900000.rapidio: port 0 lane mask 0xf is not OK [ 13.054133] keystone-rapidio 2900000.rapidio: initializing lane mask 0xf for port 0 [ 13.164087] keystone-rapidio 2900000.rapidio: port 0 lane mask 0xf is not OK [ 16.174080] keystone-rapidio 2900000.rapidio: initializing lane mask 0xf for port 0 [ 16.284072] keystone-rapidio 2900000.rapidio: port 0 lane mask 0xf is not OK [ 19.294079] keystone-rapidio 2900000.rapidio: initializing lane mask 0xf for port 0 [ 19.404073] keystone-rapidio 2900000.rapidio: port 0 lane mask 0xf is not OK [ 22.414075] keystone-rapidio 2900000.rapidio: initializing lane mask 0xf for port 0 [ 22.524073] keystone-rapidio 2900000.rapidio: port 0 lane mask 0xf is not OK [ 25.534075] keystone-rapidio 2900000.rapidio: initializing lane mask 0xf for port 0 [ 25.644069] keystone-rapidio 2900000.rapidio: port 0 lane mask 0xf is not OK [ 28.654074] keystone-rapidio 2900000.rapidio: initializing lane mask 0xf for port 0 [ 28.764073] keystone-rapidio 2900000.rapidio: port 0 lane mask 0xf is not OK [ 31.774074] keystone-rapidio 2900000.rapidio: initializing lane mask 0xf for port 0 [ 31.884073] keystone-rapidio 2900000.rapidio: port 0 lane mask 0xf is not OK [ 31.884083] keystone-rapidio 2900000.rapidio: RIO port register timeout, port mask 0x1 not ready
Please guide on this,