Hello everyone,
I'm running a simple program with openmpacc in offloading mode. So in my target code I've got something like this:
#pragma omp target data map(to:VARIABLE[0:size])
{
#pragma omp target
{ function(f1);}
}
When VARIABLE is not a pointer it compiles and runs correctly but when It is a pointer, it compiles and when running I got the following error:
"ERROR: Variables accessed via a pointer in a target region must be shaped using array sections e.g. map(to:ptr[start:size]). This is an implementation restric
tion in the current runtime and will be fixed in a future release"
1) Is there a way to map pointers like that or it is not implemented yet?
2) I also would like to know if the omp target update construct supported by TI OpenMP-acc is blocking or non-blocking?
I'm using an EVMk2h board and ti-processor-sdk-linux-rt-k2hk-evm-03.01.00.06.
I appreciate your help
Thanks