Can you please provide the following information for the V62/07648-01XE part?
Smitha,
I am requesting some data to be modeled for the Theta Jb and Jc. This should be available in a few days.
1,3 can be answered from the datasheet. Max Tj is 150c, and Max power is function of Theta and how temp is constrained ie Ja, Jb, Jc to maintain under max Tj.
Typical power is also in data sheet. Icc 10ma typ in the 1st page bullets.
I will update with other parameters when complete.
Regards,
Wade
Thank you
Here are the values:
Theta JA-High K 76.8 Theta JC, top 38.1 Theta JB 34.2 Psi JT 7.5 Psi JB 33.9
Weight: 157.2mg
thank you