Giulia,
We are moving this inquiry to the appropriate forum.
Best Regards,Chris FeatherstoneLinear Characterization EngineerHigh Performance Linear Products
Sorry for delay, as I thought someone else was replying.
The reliability report is available from the product folder.
Near the bottom : http://www.ti.com/product/opa340-ep
Or direct link:
http://www.ti.com/litv/pdf/sbok014
Regards,
Wade
Thank you. I wonder if there are any data from field or from more extensive life test. I want to use in a submarine application and a better reliability extimation is needed. Can you help me with some more info or suggesting me a different type of component that have these data available? Thanks a lot.
Giulia salmini
In the past TI has supported customer interested in using our product in undersea communication applications. In most cases they elected to use a military grade device and added additional screening, such as 100% burn-in, and additional qualification, such as a life test by wafer lot. As long as your part selection is restricted to catalog commercial-grade products, the additional options I mentioned would likely not be available.
The family data for this technology shows a failure rate of 1.9 FIT derated to +55°C which is quite good.
http://focus.ti.com/quality/docs/singlesearchresults.tsp?&templateId=5909&navigationId=11213&appType=folders&searchType=orderableOption&partialSearch=false&mtbfType=true&orderablePartNumber=OPA340MDBVTEP
I would be happy to further discuss this with you in detail.