Hi, we are referring reference designs for AFE5801, the circuit for input channels in upper left corner on page 20 in the SLOU257A user guide, "AFE5801 8-Channel Variable Gain Amplifier (VGA) with Octal High-Speed ADC". We have some questions:
1) Why do they bother with the bias connection? C56, C58 and C59 decouple it completely so it does nothing.
2) If you ever installed C102 it would short out half the primary winding of T1. This would basically render the transformer non-functional.
3) What’s the point of C57? Is this in case there’s some DC bias on the input? What would cause that?
4) Given that the input is single-ended, why have the balun at all. According to the datasheet the AFE is fine with single-ended inputs.
It looks like we should just terminate our coax with a 50R resistor and connect the signal to INP and connect INM to a 100nF to AVSS. Would you agree?
Thanks,
John