Hi, i'm using ADS5294. When i write command X"0100" to address X"28" to select bit-wise readout mode, it always turns out to be the byte-wise mode. I'm sure that the register is configured successfully because modifications to other registers work well. Has anybody successfully used the bit-wise mode for ADS5294?
Thanks very much!