hi ,
can i with the afe44xx commande 3 IR LEDs , and iF it Is a yes , how ??
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi ,
can i with the afe44xx commande 3 IR LEDs , and iF it Is a yes , how ??
thank you
Manai,
The AFE44xx devices can only control two LED's individually (more than two if you add LED's in series/parallel). If you connect the three LED's in parallel so they light up at the same time, the forward voltages may be mismatched resulting in uneven flow of current. If you connect the three of them in series, you must ensure that the LED_DRV_SUP is greater than the three forward voltages added up with some headroom of ~1V.
Regards,
Gui