I just installed the last version of AFE4400 EVM GUI, when I open the GUI the connection is established no problem with that, but once a click on capture I get this error message : "reading stopped without returning the expected number of samples. Please check the device and the inputs" then obviously it can't calculate the FFT and I get : "Insufficient number of samples for FFT calculation"
I didn't changed the device configuration.
What I noticed is that I didn't got the message box informing of a communication error and asking if I wish to continue is simulation mode. However on top right of the GUI I have simulation mode !
the driver are well installed on a Windows7 PC, on virtual com port 24
thanks for the help