Hi all,
I'm trying to implement motion cancellation in PPG signals using the AFE4400SPO2EVM. I've soldered the MPU9150 on the EVM and I'm getting the data from three axes from it along with the PPG Red and IR values from PPG sensor which I've fixed below the EVM so that we get correlated motion data.
Right now I've calculated heart rate and spo2 without any motion noise. I've also implemented a motion cancellation filter which takes in noisy ppg signal and a correlated motion signal to output corrected signal.
What I'm stuck at is how to get a motion signal from the 3 axes MPU data which is correlated with the motion noise present in the PPG signal.Can anyone help me with that??
Now I know this may not be the suitable place for this post so moderators are free to move it to a more suitable place.