Hello,
I am very new to this. Can someone tell me what does the voltage on the GUI measurement page mean, the grapgh is in Volts for the LEDs
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am very new to this. Can someone tell me what does the voltage on the GUI measurement page mean, the grapgh is in Volts for the LEDs
Viney,
Thank you for you inquiry of the AFE4400. We hope to have an answer back to you shortly.
Viney,
A single, 22-bit ADC converts the sampled LED2, LED1, and ambient signals sequentially. Each conversion provides a single digital code at the ADC output. The voltage on the GUI are the codes from the ADC converted to volts. The ADC_RDY signal goes high each time the contents of the LED registers are updated. For more information on the codes from the ADC please refer to the datasheet (link below).
http://www.ti.com/lit/ds/symlink/afe4400.pdf
Here is the link to convert codes to volts:
http://e2e.ti.com/support/applications/high_reliability/f/30/t/340964.aspx
I am seeing a lot of noise getting captured on the channels. this was not the case earlier and i use to see a very clean graph earlier. now the graph is very noisy. Could some one please let me know why is this the case?
Regards
Viney Chaddha
Hello Viney,
In order to help you debug the problem can you provide the waveform plots of the noisy data?
We have come across situations where there was power line noise riding on top of the signal of interest.
If you are also noticing the power line noise, refer to the E2E post below for few pointers to mitigate the problem.
http://e2e.ti.com/support/applications/high_reliability/f/30/p/311809/1089207.aspx#1089207
Regards
Praveen.
Praveen,
Please find attached the waveform plot. I did everything as suggested but am still getting the noise even with a very short cable. I am using DCM03 sensor to collect the data.
Regards
Viney Chaddha0654.with bat power.docx
PS: How do you insert pictures in this dialogue box
Viney,
In the waveform plot, the notch filter was not enabled. Could you repeat the experiments by enabling the 50/60Hz notch filter on the GUI?
Look at the FFT of the output data and see if the noise is spread over frequency or concentrated in a single tone or set of tones.
Regards
Praveen.
P.S. You cannot directly insert pictures. You can insert a saved image from your computer by clicking the 'Insert image' icon from the menu in the editor window.
Praveen,
After repeating with the battery powered laptop the 50 Hz noise wasn't present. If I ook at the FFT the frequency of the signal is 5 Hz and multiples of 100 Hz. What is the source of these frequencies, especially the 5Hz noise
see the graphs5125.with bat power.docx
Also why do I see a lot of DC shift in the signal?
Regards
Viney Chaddha
How do you calculate the perfusion index?