From datasheet afe5809 p8:
TGC Common-mode voltage (VCNTLP and VCNTLM) is given type 0.75V,Is there a range? and within this range will not affect analog front end performance。
thx!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
From datasheet afe5809 p8:
TGC Common-mode voltage (VCNTLP and VCNTLM) is given type 0.75V,Is there a range? and within this range will not affect analog front end performance。
thx!
We have received your question about the AFE5809 and hope to have a response back to you shortly.
Hi,
Please use 0.75V as nominal number. considering the 0 to 1.5V for VcntlM/P, we can’t make it less than 0.75V. higher than 0.75V is also not recommended due to conflicting internal circuit bias point. Of course, the device will be OK if you have some variation e.g. 10~20mV.
You can also use single ended VcntlP/M, i.e. VcntlM=GND. All datasheet specs were collected at VcntlM=GND.
Thanks!
Xiaochen