Hi TI friends,
I am designing a BCM with TI AFE4300. I have a question about VLDO:
The VLDO on AFE4300 is used to supply load cell bridge and it is spec-ed as ~1.7V. However, the load cell bridges I found so far are usually supplied with 5V voltage. A given weight will generate smaller voltage variation with 1.7V supply on a specific bridge than 5V supply. Can AFE4300 handle the bridge which usually supplied by 5V? Does AFE4300 have any requirement on load cell bridge?
Thanks & BR
Kent Wang