Hi, I'm trying to communicate Visual C++ with FTDI and then get the data into my verilog code.
I'm using MPSSE ports (A and B), but both CS pins (ADBUS3 and BDBUS3) are given values 2.4V for Low and 3,3 for High. To test it in scope is working fine(because I'm choosing the trigger threshold), but when I try to get the data in my verilog code it just see CS as High logic.
If I disconnect usb cable the CS goes to 0V.
Could somebody provide me any tips to solve it?
Thank you
Danilo Câmara