Thanx for the source code for firmware 1.3 of AFE4400SPO2EVM.
As mentioned from my previous posts, I have managed to solder MPU9150 on EVM and somehow got it perfectly working with my I2C code.
But however whenever I flash the Firmware 1.3 through CCS everything works fine, But when I try to Integrate the I2C code with the firmware I face some difficulties.
When I flash the new code the COM port of AFE4400SPO2EVM (COM95 in my case) dissapears, also there are no unknown devices in that list. Thus I cant have access to the EVM.
Do I have to make changes in the driver or anything else to get I2C working with EVM.