Dear All,
As you've likely seen from my posts on this forum I have been in the process of building a reflective pulse oximeter using the AFE4490 and a the DCM03 sensor.
Until now I used the AFE4490 which I hand-soldered on a 40-pin QFN breakout board, and then placed that on a breadboard, which I then wired to my Arduino development board's SPI interface.
However, I'm having a hard time debugging my project when it comes to figuring out what is a hardware problem and what is a software problem, since hand-soldering and breadboards could be causing problems.
My new approach is to use the AFE44x0SPO2EVM and connect the AFE4490 on that board to my Arduino board's SPI interface. This means I want to disable/bypass the MSP430 on the EVM. I want the AFE4490 on the EVM to only communicate with my Arduino for reading and writing to the registers, etc.
What is the easiest way of connecting the AFE4490 on the EVM to my Arduino development board?
Thanks!