Hi,
We are facing problem in setting register values in some board.
It gives all zero values except DIAG-REG.In some boards waveform on TXP and TXM pin shows high status or incoorect.
Please Help us ASAP.
Thanks and regards,
Santosh Pawar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are facing problem in setting register values in some board.
It gives all zero values except DIAG-REG.In some boards waveform on TXP and TXM pin shows high status or incoorect.
Please Help us ASAP.
Thanks and regards,
Santosh Pawar
Hi
We are getting TX_REF voltage 3.0v and 5.0 v in some boards.
We have also observed that only control2 reg is not setting properly(ie. bits TX_REF, TX_power down).
Other bits RST_CLK_ON_PD_ALM,EN_ADC_BYP,TXBRGMOD sete/resets properly.
Regards,
Santosh pawar
Hi,
Please find Schematic and setting file attached herewith.
CONTROL2 REG settings like TX_REF voltage is not setting properly.
CONTROL1 REG is updated as per Settings.
#define SAMPLE_256
#ifdef SAMPLE_256
#define AFE4490_CONTROL0 0x00000004
#define AFE4490_LED2STC 0x01002DC6
#define AFE4490_LED2ENDC 0x02003D06
#define AFE4490_LED2LEDSTC 0x03002DC6
#define AFE4490_LED2LEDENDC 0x04003D07
#define AFE4490_ALED2STC 0x05000000
#define AFE4490_ALED2ENDC 0x06000F40
#define AFE4490_LED1STC 0x07000F42
#define AFE4490_LED1ENDC 0x08001E82
#define AFE4490_LED1LEDSTC 0x09000F42
#define AFE4490_LED1LEDENDC 0x0A001E83
#define AFE4490_ALED1STC 0x0B001E84
#define AFE4490_ALED1ENDC 0x0C002DC4
#define AFE4490_LED2CONVST 0x0D000002
#define AFE4490_LED2CONVEND 0x0E000F41
#define AFE4490_ALED2CONVST 0x0F000F44
#define AFE4490_ALED2CONVEND 0x10001E83
#define AFE4490_LED1CONVST 0x11001E86
#define AFE4490_LED1CONVEND 0x12002DC5
#define AFE4490_ALED1CONVST 0x13002DC8
#define AFE4490_ALED1CONVEND 0x14003D07
#define AFE4490_ADCRSTCT0 0x15000000
#define AFE4490_ADCRENDCT0 0x16000000
#define AFE4490_ADCRSTCT1 0x17000F42
#define AFE4490_ADCRENDCT1 0x18000F42
#define AFE4490_ADCRSTCT2 0x19001E84
#define AFE4490_ADCRENDCT2 0x1A001E84
#define AFE4490_ADCRSTCT3 0x1B002DC6
#define AFE4490_ADCRENDCT3 0x1C002DC6
#define AFE4490_PRPCOUNT 0x1D003D08
#define AFE4490_CONTROL1 0x1E000101
#define AFE4490_SPARE1 0x1F000000
#define AFE4490_TIAGAIN 0x20000000 //0x20000000
#define AFE4490_TIA_AMB_GAIN 0x21000000
#define AFE4490_LEDCNTRL 0x22017F7F //2828 //0x22011414
#define AFE4490_CONTROL2 0x23020000 //0x23000000 // TX is kept for 4.75-5.25 V supply //0x23020000 // TX is kept for 3 V supply
#define AFE4490_SPARE2 0x24000000
#define AFE4490_SPARE3 0x25000000
#define AFE4490_SPARE4 0x26000000
#define AFE4490_SPARE5 0x27000000
#define AFE4490_SPARE6 0x28000000
#define AFE4490_ALARM 0x29000000
#define AFE4490_LED2VAL 0x2A000000
#define AFE4490_ALED2VAL 0x2B000000
#define AFE4490_LED1VAL 0x2C000000
#define AFE4490_ALED1VAL 0x2D000000
#define AFE4490_LED2-ALED2VAL 0x2E000000
#define AFE4490_LED1-ALED1VAL 0x2F000000
#define AFE4490_DIAGNOSTICS 0x30000000
#endif
Hi Amy,
We have Checked CONTROL2 REG setting by measuring TX_REF voltge at pin.
Thanks and Regards,
Santosh pawar
HI,
In some boards we are also getting some noise pulses on RX_DIG_SUPPLY pin no 31(see attached image).
That board was working properly earlier but when we tried to read register settings it stops working and now it is showing TX_REF voltage 2 volts.
Timing of these pulses varies with PRP_COUNT.
We also connect decoupling capacitor 2.2uF as per your suggestion but it is showing same problem.
Thanks and Regards,
Santosh pawar
HI,
In some boards we are also getting some noise pulses on RX_DIG_SUPPLY pin no 31(see attached image).
That board was working properly earlier but when we tried to read register settings it stops working and now it is showing TX_REF voltage 2 volts.
Timing of these pulses varies with PRP_COUNT.
We also connect decoupling capacitor 2.2uF as per your suggestion but it is showing same problem.
Thanks and Regards,
Santosh pawar
HI,
In some boards we are also getting some noise pulses on RX_DIG_SUPPLY pin no 31(see attached image).
That board was working properly earlier but when we tried to read register settings it stops working and now it is showing TX_REF voltage 2 volts.
Timing of these pulses varies with PRP_COUNT.
We also connect decoupling capacitor 2.2uF as per your suggestion but it is showing same problem.
Thanks and Regards,
Santosh pawar
Hi Amy,
We are using separate TX and RX supply. We are using Linear regulator supply.
Thanks and Regards,
Santosh pawar