Hi,
We have purchased the ultrasound transmit solution (TX-SDK-V2), and have questions regarding power supplies for it. For the +/- 50 V power (for LM96550), what should the current rating be? On the Eval Kit User's Guide, it says that +/-50 V supply needs at least 250 mA capability. But the LM96550 data sheet lists no more than 40 mA total for all of its power inputs. Can we power supplies with current rating less than 200 mA?
Another question is that for Vsubstrate (-50V), can it be the same rail as the negative rail of the +/-50V? Does it have to be a separate power supply outputting the -50V?
Sean