Hi everyone,
I want to do a small project related to measuring HR using AFE4400.
But the problem is that my received signal contain a lot of noise. I can't filter out HR pattern using these signal.
Below is my configuration for AFE4400:
Reg addr: 0x20, Value: 0x000000 //default value
Reg addr: 0x21, Value: 0x000005 //Ambient DAC 0uA, stage 2 amplify disable, stage 2 gain 0 dB, Cf= 5 pF, Rf= 10k
Reg addr: 0x22, Value: 0x018888 ///turn on LED current on LED1 and LED2, value = 26mA
Reg addr: 0x23, Value: 0x020100 //config: LED H-bridge,
My sampling rate is 100Hz. LED is LP120-2 and photo-diode: LP8894
Can you guy give me any suggestion to improve my result.
Thanks so much