Hello,
I am interested in using the AFE4300 for impedance measurements. I am not interested in its weight scale measurement capabilities.
I want to built a custom board with as few components as possible. I have been looking on your reference designs tidr119 and tidra02, which are essentially the same with regards to the implementation of the AFE4300.
I need to use this for tetrapolar measurements.
1. Can I connect the two current electrodes to any two pins between 22-27 and the two voltage measurement electrodes to any two pins between 33-38?
2. Do I need the 10M Resistors you have in tidra02 between pairs of Iout pins (R-67-63)?Do I need all of them?What is their purpose?
3. Do I need the calibration or can I get away with it and leave pins 28-31 floating?
4. What is the smallest current I can inject? Can I set this with the resistor connected between pin 20 and the capacitor on pin 19? Is it controlled by the SPI?
5. What is the highest frequency I can measure impedances with? 100kHz? 150kHz? 250kHz?
6. What is the best way to choose the gain resistor?
7. Can you send me code for an MSP430 to communicate with the AFE4300 and control the impedance measurent part of the chip?
Thank you,
Mastro