Hello all,
I have two AFE4490 SPO2 evaluation boards with me, and in each of them, I've disconnected the 0 ohm resistors and thus disabled the MSP430 on the board, connecting them to a K53 eval board microcontroller. With one of them, I succeeded in writing the code and getting the LED on the DB9 connector cable to glow, and even to get PPG data from it - but on the second board, the LED just flickers faintly (I ran the code once on both of them and the LED glowed on the non working board once - it hasn't glowed since). On the working board, I'm seeing signals on TP23 and TP17, and on the non-working board, what I see are flickers of the waveform whenever the LED blinks. Otherwise, it is low.
I also probed the pins of the afe4490 chip, and it is getting SCLK, MOSI and STE correctly, and it is also giving out the clockout at 1MHz. ADC_RDY is always low. I have pulled up RESET and AFE_PDNZ and have confirmed this at the IC pins. Ground of the board is also connected to the common ground.
Could you suggest some way to tell me whether fault is in the way I have soldered the board, or whether the board itself is at fault. I do not think it is a code issue since I have run exactly the same code on another board and got it up and running. My register setting are the default ones as given in the sample code for MSP430 and have worked before for another afe4490.
Regards,
Samyukta