Hi,
I want to use AFE4400 only as Heart rate monitor.
I went through various topics listed here regarding the same but still I have some basic queries as below -
1. Can I use ANY IR photo diode and IR photo transistor to interface with AFE4400? I know there is recommended list for such devices, but has anyone tried out others?
2. Can I use a Ear lobe sensor - normally used for heart rate monitoring to interface with AFE4400?
3. Which ADC registers I need to read to give to algorithm which calculated Heart rate? 0x2A to 0x2F? But which one are used to extract ONLY heart rate?
4. Is there any specialized algorithm to calculate heart rate or method described in Q18 of is sufficient?
5. I am connecting the IR Photo LED and photo transistor as per the schematic for EVM and block diagram is attached, is it correct?
Thanks,
Ashutosh.