I have bought the AFE4403 HREVM Watch and my main purpose is to measure the HR in offline mode.
According to the "Generic Wrist Watch Programmer's Guide" , the user can control the state machine using the wrist watch push button, even so I have some related questions :
1. Is the code that provides TI enough to get the signal HR offline?
2. How could I know the battery status?
3. How could I know if the device is really storing data in flash memory?
4. How could I know if the device is ready to transfer data through USB?
5. How could I get the data from the flash memory on the PC?, maybe with any option from the AFE4403 EVM GUI?
Best regards,
Rocío