Hi,
I am interfacing AFE4400 with CC3200 over SPI.
The AFE4400 datasheet says - The device latches data on DIN on the SCLK rising edge as per Figure 1. Serial Interface Timing Diagram, Read Operation(1)(2)(3) - - so thats SPI sub mode 0 as per SPI specs.
Now i have another SPI peripheral connected to CC3200 which has SPI sub mode 1, so eventually i can not connect these two devices together.
Any one faced such problem?
Is there any way to configure AFE4400 in other SPI mode?
Thanks,
Ashutosh.