Yesterday I came accross some very stange behaviour of a DDC112UK.
Dumping the DDC data retrieved showed the following:
(Integration time for both sides 50ms +/- 10ppm, continuous mode, DDC set to range 1)
Format:
Ch1A, Ch2A
Ch1B, Ch2B
...., ....
3782, 3636
3532, 3645
3420, 3612
3942, 3636
3162, 3613
4105, 3654
3042, 3627
4210, 3634
2888, 3638
4499, 3657
2664, 3627
4672, 3649
2376, 3620
4905, 3642
2179, 3616
5172, 3650
1988, 3604
5235, 3657
1858, 3590
5394, 3670
1782, 3624
5588, 3674
1619, 3580
5603, 3661
1539, 3618
5876, 3656
1031, 3580
6053, 3678
1288, 3631
6084, 3652
895, 3593
6219, 3670
873, 3609
6405, 3666
577, 3578
6656, 3685
439, 3608
6810, 3647
279, 3598
6925, 3676
140, 3609
7199, 3679
0, 3571
7341, 3686
0, 3615
7496, 3664
0, 3569
7636, 3690
0, 3602
7894, 3691
0, 3558
8014, 3681
0, 3612
8222, 3678
0, 3594
7275, 3702
56, 3564
7059, 3662
74, 3621
7096, 3658
111, 3621
7068, 3651
224, 3612
6950, 3659
338, 3623
6821, 3632
If channel 1 sides A and B are added, the total seem to be correct.
However it is strange to see that for channel 1 one side is decreasing to 0 wile the other side doubles and that at the same time side A and side B of channel 2 do not change.
Any idea what could be the cause?