Hi,
Our team would use TSW1400EVM and AFE5851EVM to implement our system.
And now I have the verilog source codes (ver,1.00 and 1.11), which can work with AFE5851.
For now I want to let the verilog source code work as the HSDC Pro downloading firmware.
It is means that I want to use Quartus II and convert the source code project to .rbf file.
Then use HSDC Pro to "download firmware" this .rbf file, and it can work as HSDC Pro choosing the "AFE5851_12x".
And I have the AFE5851.ini file which has the GUI settings for AFE5851EVM.
But I don't know where do I change these settings in verilog source code.
Please help me.
Kind regards,
JhinCi
Email:
JhinCiHong19901008HY@gmail.com