Hello,
Our team now is using TSW1400EVM and AFE5851EVM to implement a system.
And I have got FPGA source code(Quartus II project). (ver,1.00 and 1.11)
I also know there is .ini file for AFE5851EVM in HSDC Pro.
Now I want to let the source code working with 5851 perfectly.
How to change the setting parameters in source code and "define.vh" according to the .ini file?
I know there are "Channel Pattern", "Channel Mapping Index", "Number of bit clks in a fclk period", "Number of bits in Output format", "Number of channels in output format"...etc which are different to other ADC.
And in "define.vh" there are CONFIGxx_DEFAULT, CHANNELxx_DEFAULT and other parameters.
So how to change the source code parameters that I can work perfectly with AFE5851EVM, rather than using HSDC Pro firmware?
I have asked this question for a long time.
If there is anyone can reply me as soon as possible, I would very appreciate.
Best regards,
JhinCi.