I have some questions about the Synchronization Pulse feature in the ADS5294 ADC. We are intending use several ADS5294 ADCs in a simultaneous sampling application, including use of the built-in data decimation function. The datasheet (page 58) gives an explanation of the use of the SYNC pulse. However, I have the following questions about pulse usage:
(1) Should a single SYNC pulse be used after power-up, rather than a continuous train of SYNC pulses? (The datasheet refers to a pulse, but Figure 60 shows a continuous train of pulses.)
(2) If a train of SYNC pulses can be used, is a potential benefit of this increased robustness with respect to power-supply glitches? Are there any disadvantages to using a continuous train of SYNC pulses?
(3) Is the required SYNC pulse timing specification independent of the ADC decimation factor used?
Many thanks,
David