• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Applications » Medical & High Reliability » All Tags » DDC112
Share
Medical & High Reliability
  • Forum

Browse by Tags

Medical & High Reliability

Welcome to the Medical & High Reliability Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
DDC112
  • ADC timing
  • DDC
Related Posts
  • Forum Post: DDC112

    Nathan Jones Nathan Jones
    Hello to all, I'm new here so I hope this is the proper place for this question. I would appreciate any help you all can give me! I am currently working with the DDC112, dual current input 20-bit ADC, and had a question about the line in the datasheet (pg. 9) that says: " For the best...
    on Apr 19, 2010
  • Forum Post: Re: DDC11xEVM-PDK Kit

    Bob Benjamin Bob Benjamin
    Jan, If the 10 Meg ohm resistor is in the circuit, the signal will be reduced as the signal will be restricted by the resistance of the resistor. The resistor can also add noise. If the photosensor is connected to IN2, then remove the JP3 jumper and place a wire jumper between P9 and P10 at Z5. If...
    on Jan 3, 2012
  • Forum Post: Re: DDC11xEVM-PDK Kit

    Bob Benjamin Bob Benjamin
    Jan, I'm glad to see you are making progress. I didn't think of the power supply connection. Powering from the DDCMB is a relatively new feature, and it worked fine in initial testing. Regarding the drift, there is a small temperature drift of the DDC112 itself, but there will also be some...
    on Jan 4, 2012
  • Forum Post: Re: DDC11xEVM-PDK Kit

    Bob Benjamin Bob Benjamin
    Jan, I'm glad to hear that you are getting good results. Unfortunately we do not have any Labview code to work directly with the DDC112. Best regards, Bob B
    on Jan 11, 2012
  • Forum Post: Re: DDC11xEVM-PDK Kit

    Bob Benjamin Bob Benjamin
    Jan, Yes, the digital portion of the DDC112 responds to digital logic levels as specified for logic high and logic low as shown in the datasheet. Best regards, Bob B
    on Jan 20, 2012
  • Forum Post: Re: DDC11xEVM-PDK Kit

    Bob Benjamin Bob Benjamin
    Jan, Basically that is correct, however you need to look at table VIII in the datasheet. 0 code is actually -0.4% of full scale so you need to adjust the ratio accordingly. To get the correct ratio, you need the (output code - zero code) divided by the full scale which will be the ratio relative to...
    on Feb 3, 2012
  • Forum Post: Re: DDC11xEVM-PDK Kit

    Bob Benjamin Bob Benjamin
    Jan, I'm not sure why you are seeing two different readings unless it has something to do with the test setup. For this test I would use a voltage source with a very high value of series resistance where I know the actual current output. If you are using a photodiode as your test input, it...
    on Feb 6, 2012
  • Forum Post: DDC112 TEST Mode communication

    Benjamin Kuch Benjamin Kuch
    Hi everyone, I just get into the DDC112. A first prototype is built and I'm currently implementing the communication. This is what I did so far: Within the initialization TEST is set to HIGH and RANGE0-2 is set to 111 (Cf = 87.5pF) CLK is connectect to the 7.372800MHz microcontroller clock...
    on Apr 25, 2012
  • Forum Post: RE: DDC112 TEST Mode communication

    Bob Benjamin Bob Benjamin
    Benjamin, What we need to see is the timing of all the clocks and data as shown on an oscilloscope. You did not say the timing of the DCLK period. You must make sure that you are not shifting out data when CONV toggles. Also, all data must be shifted out before the next falling edge of DVALID. The...
    on Apr 26, 2012
  • Forum Post: RE: DDC112 TEST Mode communication

    Bob Benjamin Bob Benjamin
    Benjamin, Glad to here you are making progress. I'm not sure which type of digital filter is used for the DDC112. Basically the delta-sigma modulator oversamples the input and by doing so moves the quantization noise into the higher frequencies and the digital filter then removes the higher frequency...
    on May 4, 2012
  • Forum Post: RE: DDC112 TEST Mode communication

    Bob Benjamin Bob Benjamin
    Benjamin, You should be able to use the SPI peripheral. You just need to make sure you maintain the timing requirements for the DDC112. Best regards, Bob B
    on May 19, 2012
  • Forum Post: RE: DDC112 TEST Mode communication

    Bob Benjamin Bob Benjamin
    Benjamin, I really don't see anything obviously wrong here. Have you verified your data with a scope reading? As you are only looping through 20 bits, you should not be getting a larger value. You may have an issue passing the variable within your program. Best regards, Bob B
    on Jul 11, 2012
  • Forum Post: RE: DDC114 transient response characteristics

    Eduardo Bartolome Eduardo Bartolome
    Hi, I do not have the experience with this myself so, the following is just a guess... I think a portion of the transient current from the photodiode will flow into the feedback capacitor of the integrator (where you expect it to go) and a portion into the parasitic capacitance of the photodiode...
    on Mar 15, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use