• Not Answered

ADS1258-EP: ADS1258-EP

Part Number: ADS1258-EP

Hello,

We are using the ADS1258 in one of our product. A transorb is connected on the ADC input line, we will test each and every production board. This testing is in power off condition. Because of the transorb testing, as per simulation we see a voltage of 30Vdc for 60mSec on ADC input line in powered off condition. However I read in the datasheet that there is a ESD diode to protect the ADC input line.

Please let us know, if the 30Vdc on ADC input line is safe and will not effect the ADC functionality.

3 Replies