This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sn55113: compatible sn55113 parts

Part Number: sn55113

I have the sn55115 on an existing system and would like a lower Icc part for the sn55113 driver that I need to replace and would be compatible. Do you have a suggestion?

3 Replies

  • Is the sn55183 compatible? or can I use an RS422/RS485 driver?
  • In reply to Frank Wadas:

    Frank,
    I am taking a look at this, and will reply back.
  • In reply to Wade VonBergen:

    Frank, on the surface it looks like the SN55183 could be compatible.
    Though it would be helpful to have some more information.
    Is this single receiver single driver on media?
    What is media, distance, frequency?
    What termination?
    RS422/485 devices may also work.

    The receiver has very large common mode, so as long as the driver can drive the load at frequency with appropriate differential, then it should work well.
    Regards,
    Wade

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.