• Resolved

LM119QML: Test Conditions details

Part Number: LM119QML


I  don't understand the conditions of electrical characteristics of LM119 (SNOSBJ2B) datasheet p 5.

 In line 1, for Input Offset Voltage, what is the resistance Rs which is less or equal of 5K ? Is it the impedance in series with inputs ?

In line 12, for Saturation Voltage, what is the voltage Vin which is less or equal of -6mV with V+ >= 4.5V and V-=0V ? Is it the common mode ?

Is there an application note with all tests circuits ?

Best regards,