Hi,
I am trying to use a TPS62000-HT part, and I cannot go above 175C without the duty cycle narrowing to an unusable value. Everything works fine up to that point, but beyond that temperature the duty cycle continues narrowing until the output voltage drops way off from its regulated value. I have tried two different board layouts in hopes that would help, but the behavior is identical in both circuits. It almost seems like the part is going into current limit, but I am only running a 3.3V output into a 50 ohm load. The part should handle that, right? Attached is the output trend with temperature. Any suggestions would be greatly appreciated.
Thanks,
Shawn