Hi Wade,
I used two days to study the datasheet of THS788, but I still have following question. Could you help me to solve these questions?
If yes, refer to the Table 22, the max time range of the course counter should be 14.31s, then, how to derive the value of interface max value?
If not, how to get the max value of the interface range?
The statement is “The THS788 allows one clock cycle, (r) for the host to reverse the data-channel direction and begins driving the Hdata line on the falling edge of HCLK pulse 12.” which is not consistent to the waveform in Figure. 3 Read Operation. Should the value of ‘12’ be ‘11’?
Thank you
Po Yuan