Hello,
i plan to use two THS788 chips in parallel, since i require 8 event channels. Both chips would share one Sync input via a fanout. My measurements will use relatively few Sync pulses (approximately one per second), but much higher rates on the event channels (>100k per second).
I'm afraid that the simple scheme of using a fanout to split the Sync pulse is not good enough to get the best possible performance. Due to the fanout's jitter and and the finite accuracy of the THS788, one chip might measure the Sync pulse 13 ps earlier or later compared to the other chip. Then all measurements until the next Sync pulse will be systematically off by +- 13ps.
Is there a possibility to avoid this problem? If one could access the current Sync time stamps it would be easy to correct for this problem, by checking that the lowest 6 bits of the two sync time stamps always have a fixed difference.
Regards,
Markus