Hello Team,
I have a customer who is experiencing additional 400ns of deadtime added to the duty cycle after the oscillator starts its charging cycle. The output pins do not go high until 440ns after the oscillator starts the charging cycle. Below is detailed on what the customer is facing :
" We’re using a push pull topology, but I tested the chip open loop by itself as well. We tested with various values. This is not the dead time as described in the datasheet. This is after the deadtime occurs and the oscillator starts to charge back up. The delay remains about 400ns (in addition to the deadtime determined by the Ct) regardless of the timing parts, after the deadtime should have ended.
We tested on a PCB with 1nF & 6.98k; 1.3nF & 5.23k. Additionally tested with 1nF and 4.7nF on a breadboard, with a pot for Rt. The Ct is very close to the pin on the PCB. We are using NP0 caps.
Is there any way to get any schematics or anything on this chip? We keep running into problems with the datasheet, it is full of errors and missing information.
In the simulation reference design, this issue does not occur, the output fires as soon as the dead time is over and the charging cycle of the oscillator starts. This issue is not modeled in the sim.
Also please let me know regarding the schematics, as I’ve said it is frustrating to keep finding new mistakes and omissions in the datasheet. Thanks for looking into it. "
I could find much information other then thinking this might have to do with the oscillator in use. Could you point us to the correct direction towards resolving this issue.
Thank you for your time.
Sincerely,
Kishen