Do you have any guidance for what to do with unused analog inputs for the ADS1282-SP? Is there a termination/protection scheme that you would recommend?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do you have any guidance for what to do with unused analog inputs for the ADS1282-SP? Is there a termination/protection scheme that you would recommend?
Hi Steve,
Page 17 of the datasheet states the following:
The specified input operating range of the PGA is shown in Equation 2:
AVSS + 0.7 V < (AINN or AINP) < AVDD – 1.25 V (2)
Absolute input levels (input signal level and common-mode level) should be maintained within these limits for
best operation.
So long as the unused input meets the bias condition of equation 2, the circuit will be OK.
Thanks,
Christian